cancel
Showing results for 
Search instead for 
Did you mean: 

Output voltage characteristics of STM32G070CB

Kraal
Lead

Hello folks,

I can't figure out the meaning of table 48 p.64 of STM32G070CB datasheet (see attached picture). In particular the FT_c pins. Page 63 it is written that all I/O can source up to +-6mA and +-15mA with relaxed VOL and VOH.

Back to table 48, FT_c pins can have +-2mA or even +-1mA Iio as conditions, but I fail to understand the differences between the lines (1 & 2) and lines (7 & 8).

Pratical case: if I want to use PD0 (FT_c) to generate a PWM to drive a MOSFET, what will be the maximum current output of this pin ? Vcc is 3.3V.

Thank you very much,

Kraal

0693W00000WJismQAD.png

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Bubbles
ST Employee

Hello @Kraal​,

it's not obvious, but not too difficult either. lines 1&2 are under condition VDDIO > 2.7V. The lines 6&7 are for lower voltages, basically starting at BOR voltage threshold.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

sorry I meant 7&8 of course

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you @JHOUD​ for this clarification.

Now regarding the practical case, what is the output current of FT_c pins in PWM output when driving a MOSFET ?

Best regards,

Kraal

Hi @Kraal​,

that only depends on the load, which is the MOSFET in this case. I'm more SW oriented, but from what I remember the MOSFET gate is controlled by voltage, not current. I expect the gate impedance to be pretty high. Check the DS of the MOSFET you want to use, or run some simulation if model is available.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.