cancel
Showing results for 
Search instead for 
Did you mean: 

Optical SPDIF - MCU takes as input - Process - Output the SPDIF signal

Basit009
Associate

Hi,

I need help in selecting a MCU which takes optical SPDIF as an input (coming from a source like TV) and be able to process the data by applying some algorithm and then output the data over optical SPDIF. Any reference or evaluation board recommendation?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LCE
Principal II

Several STM32 MCUs have an extra "SPDIFRX" peripheral, most of their SAIs (serial audio interface) have an SPDIF TX option (I use that a lot for audio debugging, quite easy to use).

The main problem might be to retrieve and use the SPDIF RX source clock, I have never tried that, but from my experience that might cause the biggest trouble. (I like to use a sample rate converter.)

Which MCU you will finally use might also depend on how heavy the audio processing will be and the sampling rate. That's why I would start with an F7 or H7 Nucleo board.
Connecting optical IO to a Nucleo is not that hard, as it's usually only 3 pins (signal, VCC, GND).