cancel
Showing results for 
Search instead for 
Did you mean: 

Only one qspi flash connected to BK2_IOx pins of the STM32F446.

Asantos
Senior
Posted on April 21, 2015 at 02:21

Hi,

  I connected only one qspi flash to the BK2_IOx pins of the STM32F446. Is it possible to use this flash as single-flash mode? 

   Based on the STM32F446 datasheet, there's no QUADSPI_BK1_IO2 for 64 pins package, is it correct? 

    

Ari.
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 04, 2015 at 15:49

 Hi Ari,

1- To use one flash as single-flash mode, you can connect flash memory to BK1_IOx or BK2_IOx pins and select the FLASH memory to be addressed in single flash mode in the FSEL bit in QUADSPI control register (QUADSPI_CR).

2- For the LQFP64 package, the Quad SPI is available with limited features, so it is correct: there is no QUADSPI_BK1_IO2.

Sorry for answer delay ;)

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.