Skip to main content
WMcKi.1924
Associate II
May 19, 2020
Solved

On the stm32l486 the port GPIOG, pins 3-15 do not appear to be working when configured as outputs

  • May 19, 2020
  • 6 replies
  • 1925 views

I have a new product using the stm32l486, and the GPIOG pins mentioned in the title do not appear to work as outputs, even though they are configured identically to the GPIO pins I am using for ports A-F. I cannot find anything in either the datasheet or the user manual about any pecularities to port G. But when pins in the GPIOG.ODR are set to '1' they definitely do not go high, and they are still read back as '0' on GPIOG.IDR. I also do not see anything in the errata for the stm32l486. I am correct in thinking that port G works like the other ports on this part?

This topic has been closed for replies.
Best answer by waclawek.jan

Oh, and I forgot - read 5.1.2 Independent I/O supply rail in RM:

After reset, the I/Os supplied by V DDIO2 are logically and electrically isolated and therefore

are not available. The isolation must be removed before using any I/O from PG[15:2], by

setting the IOSV bit in the PWR_CR2 register, once the V DDIO2 supply is present.

JW

6 replies

waclawek.jan
Super User
May 19, 2020

These pins are powered by VDDIO2. Do you have VDDIO2 properly connected?

Not very conspicuously, but it's said both in DS (these pins are marked with suffix _s (or _fs) in the pin definitions table, with the explanation at beginning of the table) and RM (in PWR/Power supplies chapter:

V DDIO2 is the external power supply for 14 I/Os (Port G[15:2]). The V DDIO2 voltage level

is independent from the V DD voltage and should preferably be connected to V DD when

PG[15:2] are not used.

JW

WMcKi.1924
Associate II
May 19, 2020

Our board has VDDIO2 connected to VDD. So G[15:2] should be working, correct?

waclawek.jan
waclawek.janBest answer
Super User
May 19, 2020

Oh, and I forgot - read 5.1.2 Independent I/O supply rail in RM:

After reset, the I/Os supplied by V DDIO2 are logically and electrically isolated and therefore

are not available. The isolation must be removed before using any I/O from PG[15:2], by

setting the IOSV bit in the PWR_CR2 register, once the V DDIO2 supply is present.

JW

WMcKi.1924
Associate II
May 19, 2020

Yep, that's my problem. Needed to hit RCC_APB1ENR1_PWREN in RCC->APB1ENR1 and IOSV in PWR->CR2. Thank you very very much. I'm seeing mentions of those pins in the data sheet now. Thank you also for pointing that out and for the prompt and accurate response.

--b

WMcKi.1924
Associate II
May 19, 2020

I don't see a close button on this page. How do I close this request?

Tesla DeLorean
Guru
May 19, 2020

On L4+ we have this in SystemClock_Config()

 __HAL_RCC_PWR_CLK_ENABLE();
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST); /* Enable voltage range 1 boost mode for frequency above 80 Mhz (L4+) */
 HAL_PWREx_EnableVddIO2(); /* IOSV bit MUST be set to access GPIO port G[2:15] */
 __HAL_RCC_PWR_CLK_DISABLE();

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..