cancel
Showing results for 
Search instead for 
Did you mean: 

On stm32h753 eval board, which uart is connected to ST-LINK version 3?

DSwar.2
Associate II

I would like to be able to write debugging messages to a serial terminal. Is there sample code that does this? Is there something I need to know about setting up clocks that is special for ST-LINK v3? How does one know which uart is connected to ST-LINK? Is it on pin PF9?

1 REPLY 1

>>Is it on pin PF9

No

And the PG9/PG14 connections are on the ST-LINK IC, not the H753

That would be EVAL2 (MB1246 RevE) board, there should be jumpers to allow selection between RS232 connector or the ST-LINK, on USART1

JP7 / JP8

PB14 / PB15

https://www.st.com/resource/en/user_manual/um2198-evaluation-boards-with-stm32h743xi-and-stm32h753xi-mcus-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..