cancel
Showing results for 
Search instead for 
Did you mean: 

NWE pulse problem

nugoori72
Associate II

I want use external memory IC(IDT 7204 FIFO memory)

I use two STM32H743II(one is write FIFO, one is read FIFO)

I think read was good work.

but write is not good.

I set FMC LCD Interface like Cubeset picture

I think one data write operation, NWE pulse appear 1 time.

but when one data write, 4 NWE pulse shown.(refer tek0009 scope data)

write code is like below.

*(__IO uint16_t *) FIFO_D = rCnt;

4 NWE pulse is normal status?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

All signals for static memories and similar parallel interfaces are qualified by the NEx (chipselect) signal, so you should observe also that signal.

JW

nugoori72
Associate II

NE1 is two pulse.

why 2 pulse?

waclawek.jan
Super User

Well, I don't know.

Does the address/data remain the same, i.e. does it write the same data to the same address twice? If yes, it can't be considered an error - static memories wouldn't care about it, it's just ineffective. It even may be documented - look into the errata.

JW