cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo32 Sleep

maryam magdy
Associate II
Posted on March 10, 2018 at 18:53

Hello,

I have the Nucleo L43KC MCU. Is there any way I can put it into sleep or standby or other power modes? I noticed it doesn't have a wakeup pin unfortunately after I bought it

Thanks

1 REPLY 1
Tilen MAJERLE
ST Employee
Posted on March 12, 2018 at 09:49

Hello

maryam.magdy

‌,

http://www.st.com/en/evaluation-tools/nucleo-l432kc.html

has STM32L432 MCU which is based on standard STM32L4 technology.

http://www.st.com/content/ccc/resource/technical/document/application_note/9e/9b/ca/a3/92/5d/44/ff/DM00148pdf/files/DM00148pdf/jcr:content/translations/en.DM00148pdf

gives you overview of low-power features on this MCU.

Hardware wake-up pin is available on PA0 and PA2 pins. Please refer to AN46 You will see the options to wakeup MCU.

Best regards,

TIlen