2018-03-10 09:53 AM
Hello,
I have the Nucleo L43KC MCU. Is there any way I can put it into sleep or standby or other power modes? I noticed it doesn't have a wakeup pin unfortunately after I bought it
Thanks
2018-03-12 01:49 AM
Hello
maryam.magdy
,http://www.st.com/en/evaluation-tools/nucleo-l432kc.html
has STM32L432 MCU which is based on standard STM32L4 technology. gives you overview of low-power features on this MCU.Hardware wake-up pin is available on PA0 and PA2 pins. Please refer to AN46 You will see the options to wakeup MCU.
Best regards,
TIlen