cancel
Showing results for 
Search instead for 
Did you mean: 

[ NUCLEO-L552ZE-Q ] Why "EXTI Line 14 interrupt " not "EXTI line 13 interrupt"?

MQi.1
Senior II

I tried this tutorial"https://www.stmcu.com.cn/ecosystem/chip/chipfamily-STM32L5-4", it was not in English. bu the illustration is clear, I tried it in STM32CubeIDE version 1.4.0 on Ubuntu 20.04.1 LTS. When I went to the last step - Setting NVIC_S and NVIC_NS, it was "EXTI Line 14 interrupt" there, not "EXTI Line 13 interrupt", I used NUCLEO-L552ZE-Q board(https://ibb.co/yNtQxDF), there was a pushbutton in EXTI line 13, so if there wasn't it, the button would be no way for using, how to add it or maybe this was just a typo?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

Maybe you've chosen some other pin than PC13 for EXTI?

JW

MQi.1
Senior II

Before, I have just set LPUART1 with PG7 and PG8 for RX and TX default.

MQi.1
Senior II

You are right, I have just reload the .ioc file, and altered PC13 in "Pinout view" from "PWR_WKUP2" to "GPIO_EXIT13", then in "Connectivity-->LPUART1-->NVIC_NS Interrupt Table" enabled it. Then, in "System Core--> NVIC_NS and NVIC _S" there is "EXIT LINE 13 interrupt".