cancel
Showing results for 
Search instead for 
Did you mean: 

Keeping PA15 low during the init

Akshit Singhal
Associate II

Hi community,

I'm using STM32F303RE, in that I'm using PA15 as a GPIO which is connected to a Relay, but I recently found out that the PA15 is a JTDI pin which is being pulled up internally, so whenever the STM32 resets, it gets high and after GPIO_init is executed it goes lows. It's causing relay trigger.

Kindly help!

Regards

Akshit Singhal

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

You can't change the behavior of PA15 on reset. Use a different pin with an external pulldown.

If you feel a post has answered your question, please click "Accept as Solution".