2016-09-17 05:55 AM
Hello,
I would like to develop with the STM32L476RG and I have tried a few IDE without success. Everything is up to date.Building the project fails with KEIL :*** Using Compiler 'V5.06 update 3 (build 300)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'xxxxxx'FCARM - Output Name not specified, please check 'Options for Target - Utilities'Target not created.Build Time Elapsed: 00:00:00Building the project fails with SW4STM32. I have found a workaround (modify .ld : ''RAM1'' to ''RAM'').Building the project fails with TRUESTUDIO (same error as SW4STM32). Same workaround (modify .ld).I suspect that CubeMX simply doesn t not produce working project for this chip.KR.Patrick.2016-09-19 05:53 AM
Hi pdu-fr,
I subbmit you feedback to our CubeMx team for investigation. Thanks. -Hannibal-