cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-L476RG + CubeMX 4.16.1 + FW L4 1.5.1 + Keil uVision5.21

pdu-fr
Associate II
Posted on September 17, 2016 at 14:55

Hello,

I would like to develop with the STM32L476RG and I have tried a few IDE without success. Everything is up to date.

Building the project fails with KEIL : 

*** Using Compiler 'V5.06 update 3 (build 300)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'

Build target 'xxxxxx'

FCARM - Output Name not specified, please check 'Options for Target - Utilities'

Target not created.

Build Time Elapsed:  00:00:00

Building the project fails with SW4STM32. I have found a workaround (modify .ld : ''RAM1'' to ''RAM'').

Building the project fails with TRUESTUDIO (same error as SW4STM32). Same workaround (modify .ld).

I suspect that CubeMX simply doesn t not produce working project for this chip.

KR.

Patrick.

1 REPLY 1
Walid FTITI_O
Senior II
Posted on September 19, 2016 at 14:53

Hi pdu-fr,

I subbmit you feedback to our CubeMx team for investigation.

Thanks.

-Hannibal-