cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-L476 HSI configuration

Posted on April 23, 2018 at 07:53

I use Stm32cubemx generate code with nucleo-l476 board.it run well if i use sw4stm32, but if i compile it using Clion with gcc, it will hand in HAL_RCC_ClockConfig(). After debugging and searching, i found the reasion should be missing one line.

 origin is :

 /**Initializes the CPU, AHB and APB busses clocks 

    */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  

RCC_OscInitStruct.HSICalibrationValue =16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

  RCC_OscInitStruct.PLL.PLLN = 10;

  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;

  RCC_OscInitStruct.PLL.PLLQ =

RCC_PLLQ_DIV2

;

  

RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

it should be :

 /**Initializes the CPU, AHB and APB busses clocks 

    */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  

RCC_OscInitStruct.HSICalibrationValue =16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

  RCC_OscInitStruct.PLL.PLLM = 1;

  RCC_OscInitStruct.PLL.PLLN =

10;

  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;

  RCC_OscInitStruct.PLL.PLLQ =

RCC_PLLQ_DIV2

;

  

RCC_OscInitStruct.PLL.PLLR

=

RCC_PLLR_DIV2;

is it a bug? or because my poor knowledge?

8 REPLIES 8
Posted on April 23, 2018 at 09:04

It is a bug in CubeMX that has been reported/described numerous times, hopefully it will be fixed in 4.26

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
Lead II
Posted on April 23, 2018 at 10:36

Hello

hiwszjq

,

As said by Clive, this is an issue on CubeMX version 4.25: The

PLLM parameter

is not generated for the STM32L4 MCUs.

This is already reported internally and will be fixed in the next releases of CubeMX.

Sorry for any inconvenience this may have caused.

Khouloud.

Posted on April 23, 2018 at 09:18

but i can't find solution on google & baidu(Chinese Searching Engine), and i just start to learn STM32.

Nawres GHARBI
ST Employee
Posted on April 23, 2018 at 15:10

Hi Zhou 

This will be fixed next release. As a workaround, you can use the RCC LL Driver where the PLLM is well configured..

Posted on April 23, 2018 at 15:26

thankyou.i will try it

Posted on April 23, 2018 at 17:12

Just paste in the missing line, as needed, or run without PLL if you're continually rebuilding with CubeMX

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 07, 2018 at 09:58

the 4.25.1 will be available this week fixing this issue, stay tuned 

Khouloud GARSI
Lead II