cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo L053 & IDB04A1 & IDB002V1

eleventen
Associate III
Posted on December 24, 2014 at 03:02

We're looking to evaluate the Nucleo STM32L053 with the BlueNRG shield.  On hand, we also have the IDB002V1 eval kit for the BlueNRG.

We're following the documentation in AN4559 to evaluate the SensorDemo program.  A couple of questions came up almost right away.

1) There are two SensorDemo applications.  One is called SensorDemo and the other is called SensorDemo_GATTServer.  Which one is being evaluated in chapter 6 of the app note?

2) While we don't have the IDB003 dongle, we do have an IDB002v1 which ought to let us do the same things as the dongle.  We're following the directions in the app note and find that when we try to execute BLUEHCI_GAP_START_GEN_DISC_PROC, the status is 0xc for Command Disallowed.  What would cause this response? 

Thoughts?

2 REPLIES 2
eleventen
Associate III
Posted on December 24, 2014 at 04:03

We updated the IDB002 to the 6.0 version of the GUI.  This changes the behavior quite a bit.

As requested by the GUI, we updated the motherboard to firmware 1.4 and the BlueNRG to 6.4  The new UI has scripted initialization and scanning features.  Now, the scanning command succeeds.  Which is good.  Yet now we don't see how to take the results of the scanning and connect to the Nucleo running the SensorDemo.

Thoughts?

markbewley9
Associate
Posted on February 04, 2015 at 21:44

Does any know where to get sample IAR code for the STM32L151 on the IDB002V1? 

Thanks