cancel
Showing results for 
Search instead for 
Did you mean: 

Which CubeMX packages should be installed?

Andrei Chichak
Lead II
Posted on January 26, 2015 at 23:25

Are the cube firmware packages cumulative?

Version STMCubeF4 1.4.0 came out recently, but I noticed that version 1.2.0 is significantly smaller than 1.1.0 or 1.3.0. This hints that all of the packages should be installed since they don't seem to be cumulative (or the size would just keep on increasing).

So, should I install all of the versions or just the latest?

Thanks
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on February 04, 2015 at 19:24

Hello,

These releases are not cumulative (only patch releases are. Patch release for 1.4.0 would be 1.4.x where x>=1). 

When working on a project through STM32CubeMX tool: the latest firmware package release compatible with the tool will be proposed for download (automatically if the release is not already available in your local Cube repository).

Best regards

Best regards