2023-02-16 10:44 AM
I'm trying to do a quick eval of a NUCLEO-G474re board for use of the SoC as a product communication controller (I2C, SPI, RS-485, etc.), initially using the Arduino environment for rapid testing. Initial attempt to bring up I2C causes NO activity on SCL/SDA as observed on a logic analyzer.
Relevant code fragments for a DS1683 at 7-bit address 0x6B:
#include <Wire.h>
Wire.begin(); // SCL/SDA on Arduino D15/D14 (G474 PB8/PB9)
Wire.setClock(100000L); // 100 kHz
Wire.beginTransmission(0x6B);
Wire.write(0x01); // Check the Status register
Wire.requestFrom(0x6B, 1);
byte RegData = Wire.read();
Wire.endTransmission();
Am I missing something obvious? Why is the I2C bus quiet?
Thanks!
Edit: Downloaded an I2C Scanner sketch. No I2C activity on the NUCLEO, but works on an Arduino Due.
-BobC
Solved! Go to Solution.
2023-02-17 5:54 AM
Hello @BCunn.1 ,
You can refer to this article : STM32 Arduino (STM32duino) Tutorial (site.com)
#include <Wire.h>
void setup() {
Wire.begin();
Serial.begin(9600);
Wire.setClock(100000);
Wire.beginTransmission(deviceAddress); // get the sensors attention
Wire.write(registerAddress); // move your memory pointer to registerAddress
Wire.endTransmission(); // completes the ‘move memory pointer’ transaction
int data = 0;
}
void loop() {
Wire.requestFrom(deviceAddress, 1); // send me the data from the register
data = Wire.read(); // data from registerAddress
Serial.println(data); // print the reading
}
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-17 5:54 AM
Hello @BCunn.1 ,
You can refer to this article : STM32 Arduino (STM32duino) Tutorial (site.com)
#include <Wire.h>
void setup() {
Wire.begin();
Serial.begin(9600);
Wire.setClock(100000);
Wire.beginTransmission(deviceAddress); // get the sensors attention
Wire.write(registerAddress); // move your memory pointer to registerAddress
Wire.endTransmission(); // completes the ‘move memory pointer’ transaction
int data = 0;
}
void loop() {
Wire.requestFrom(deviceAddress, 1); // send me the data from the register
data = Wire.read(); // data from registerAddress
Serial.println(data); // print the reading
}
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.