2024-06-16 07:29 AM
Hello,
I have connected the nucleo f756zg board with the qorvo dwm3000. I found the inc and src files for the dwm3000 but the drivers for the dwm3000 are available for the m33 and m4 families.
Is it someone who used an M7-Cortex mcu and have the driver for the dwm3000? Or, is there any other way to go?
Thank you in advance,
Dim
2024-06-16 08:42 AM
If you've got the source files, port it. Work with the vendor their FAE's or consultants.
CM4 code should run on a CM7
Related to these?
https://community.st.com/t5/stm32-mcus-embedded-software/dw3300q-stm32-sdk/td-p/676724
2024-06-16 12:31 PM
Here you can find help with adaptation or development of the driver.
2024-12-14 07:14 AM
In qorvo software package for DWM3000, they have provided a stm32 project, but it has been initiated for STM32F429 Nucleo board. I have STM32F446 Nucleo board, so how can i port that project to use with my nucleo board.
Thanks in Advance !
2024-12-14 07:22 AM
You'll need to start by identify the pins/peripherals used on the STM32F429I-DISCO board, and change those to available equivalents on the NUCLEO-F446 which are free