2016-09-30 9:28 AM
&sharpdefine SAMPLESDAC (1024*2)
static TIM_HandleTypeDef Timer4Handle;void Timer4_init(){ TIM_ClockConfigTypeDef TimerClockConfig; TIM_MasterConfigTypeDef sMasterConfig; __TIM4_CLK_ENABLE(); //Timer init Timer4Handle.Instance = (TIM_TypeDef *)TIM4; Timer4Handle.Init.Prescaler = 0; Timer4Handle.Init.CounterMode = TIM_COUNTERMODE_UP; Timer4Handle.Init.Period = 108; Timer4Handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; //Timer4Handle.Init.RepetitionCounter = 0; //Timer4Handle.Channel = HAL_TIM_ACTIVE_CHANNEL_1; //Timer4Handle.hdma[0] = &DMA_ADC_Handle; HAL_TIM_Base_Init(&Timer4Handle); TimerClockConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; HAL_TIM_ConfigClockSource(&Timer4Handle,&TimerClockConfig); sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; HAL_TIMEx_MasterConfigSynchronization(&Timer4Handle, &sMasterConfig); //HAL_TIM_Base_Start(&Timer4Handle); HAL_TIM_Base_Start_IT(&Timer4Handle);}static DMA_HandleTypeDef DMA_DAC_Handle;static DAC_HandleTypeDef DacHandle;void dac_init(){ // we assume AnalogIn has configureed GPIO, we need ADC channel ? __DAC_CLK_ENABLE(); // Enable ADC clock // Configure ADC DacHandle.Instance = (DAC_TypeDef *)DAC; //DacHandle.DMA_Handle1 =&DMA_DAC_Handle; HAL_DAC_Init(&DacHandle);}void dma_dac_init(){ // DMA init ADC1 is DMA2 channel0 stream 0 or 4 use DMA2_Stream0 thd __DMA1_CLK_ENABLE(); DMA_DAC_Handle.Instance = DMA1_Stream6; //DMA_DAC_Handle.State = HAL_DMA_STATE_READY; //HAL_DMA_DeInit(&DMA_DAC_Handle); DMA_DAC_Handle.Init.Channel = DMA_CHANNEL_7; DMA_DAC_Handle.Init.Direction = DMA_MEMORY_TO_PERIPH; DMA_DAC_Handle.Init.PeriphInc = DMA_PINC_DISABLE; DMA_DAC_Handle.Init.MemInc = DMA_MINC_ENABLE; DMA_DAC_Handle.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; DMA_DAC_Handle.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; DMA_DAC_Handle.Init.Mode = DMA_CIRCULAR; DMA_DAC_Handle.Init.Priority = DMA_PRIORITY_VERY_HIGH; DMA_DAC_Handle.Init.FIFOMode = DMA_FIFOMODE_DISABLE; DMA_DAC_Handle.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; DMA_DAC_Handle.Init.MemBurst = DMA_MBURST_SINGLE; DMA_DAC_Handle.Init.PeriphBurst = DMA_PBURST_SINGLE; HAL_DMA_Init(&DMA_DAC_Handle); __HAL_LINKDMA(&DacHandle, DMA_Handle2, DMA_DAC_Handle);}void dac_readn( uint16_t * data, uint32_t nelems){ DAC_ChannelConfTypeDef sConfig; sConfig.DAC_Trigger = DAC_TRIGGER_T4_TRGO; // Timer6 as triger sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE; HAL_DAC_ConfigChannel(&DacHandle, &sConfig, DAC_CHANNEL_2); HAL_DAC_Start_DMA(&DacHandle, DAC_CHANNEL_2, (uint32_t *)data, nelems, DAC_ALIGN_12B_R); //while (DMA_DAC_Handle.Instance->CR & DMA_SxCR_EN); // spin //HAL_DAC_Stop_DMA(&DacHandle,DAC_CHANNEL_1);}void SawToothWave(){ int i = 0; for(; i <= SAMPLESDAC; i ++) { DAC_Val[i]=1024+i; //DAC_Val[i]=2048; }} #dac-bug2016-09-30 9:36 AM
int main()
{ Timer4_init(); SawToothWave(); Timer6_init(); dac_init(); dma_dac_init(); dac_readn(DAC_Val,SAMPLESDAC);//Followed by large noise while (true) { led1 = !led1; Thread::wait(500); }}/************************************************************/
If i call as the above code , it optput SAW UP signal followed by large noise,When i do a strange code bellow, it output SAW UP signal correctly.int main(){ Timer4_init(); SawToothWave(); Timer6_init(); dac_init(); dma_dac_init(); dac_readn(DAC_Val,SAMPLESDAC-512);//correct SAW UP signal while (true) { led1 = !led1; Thread::wait(500); }}2016-09-30 9:38 AM
Why I must leave 512 point in DMA to get a correct waveform?
2016-09-30 9:42 AM
correct waveform with 512 point off.
________________ Attachments : graphs_ok.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzwz&d=%2Fa%2F0X0000000bRP%2F_FRFm6o6yxa8qo9krz9r3423EtBIfTVludvykMfgZuc&asPdf=false2016-09-30 9:44 AM
Wrong waveform , but code is understandable.
________________ Attachments : graphs.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzwu&d=%2Fa%2F0X0000000bRO%2Fq4oARtUmBjunBj96AN8CoEQr9jRM6o4zHJohvJEqN98&asPdf=false2016-09-30 11:17 AM
You can edit/amend your own posts...
Code still incomplete, when trying to demonstrate a failure provide a complete example that will compile.Is the pattern buffer placed in non-cached memory?