2023-03-29 6:10 PM
[Update]
Seems you can't mix C and C++ files easily, so I converted the main file to C and everything works fine.
[/update]
I am attempting to do what I thought would be a simple pin change interrupt on PB0.
I set up the pin change in HAL and it works, I do it in my C++ project and it doesn't. The registers look the same but I don't see what the problem is. I've been chasing it for hours.
I have a debounced external button, tested with other processors and with this board and HAL and it works as advertised.
The button is wired to pin CN10 34 @ 5V
void EXTI0_1_IRQHandler (void)
{
EXTI->RPR1 |= 1;
}
int main(void)
{
// Enable GPIOB clock
RCC->IOPENR|= RCC_IOPENR_GPIOBEN;
// Enable SYSCFGEN
RCC->APBENR2 |= RCC_APBENR2_SYSCFGEN;
// Configure PB0 as output with pull down
GPIOB->MODER &= ~(3 << 0);
GPIOB->PUPDR |= 2;
// External interrupt select PB0
EXTI->EXTICR[0] |= EXTI_EXTICR1_EXTI0_0;
// wakeup with interrupt unmasked PB0
EXTI->IMR1 |= EXTI_IMR1_IM0;
// Rising edge select
EXTI->RTSR1 |= EXTI_RTSR1_RT0_Msk;
NVIC_SetPriority(EXTI0_1_IRQn, 1);
NVIC_EnableIRQ(EXTI0_1_IRQn);
/* Loop forever */
for(;;);
}
Any help appreciateed.
2023-03-29 9:18 PM
Check IRQ_Self_Setlle.c here
The demo that runs on STM32C0316-DK enables MCO and by manually injecting it to an EXTI input pin to flood and swamp the core with interrupts. The demo countermeasure use a HW Timer to limit the core workload to avoid what would be similar to a DDOS attack-like.