2015-06-08 8:04 PM
Hi everyone,
I have a STM32F072B Nucleo board (god knows why, should have listen to good advises -.-) and IAR Workbench with the 32Kb code limit version. V7.40.In an attempt to get more familiar with IAR tools I was looking for ways to monitor data in a graphic and monitor code execution cycles.So I tried to use the tools under ''ST-Link''.First what it seemed easier. Data logging. I configured the SWO to know the target is at 48Mhz and the SWO clock to 2000Khz. Opened the data log window, added the variable I wanted and waited... for nothing. There is no data getting into the graph.I am not sure if I did anything wrong, all my drivers are installed, I tried also using the SWO trace (after some messing arround with the config) and nothing happens.Could this be because of the dam Nucleo board or am I doing something wrong?Help is really appreciated as I tried for quite a while to search for info on this but it seems everything I am doing is correct (obviously there is something wrong with either my steps or the board)2015-06-09 4:43 AM
Hello Afonso,
The Data logging that you want enable is the Power Log Setup window?If not, could you sent a print screen of this window?2015-06-09 9:49 AM
2015-06-09 10:26 AM
Don't Cortex-M0 parts have very limited SWO functionality?
2015-06-09 10:50 AM
Afonso,
I develop in IAR and never saw this window, but if you find some figure in web poste here.Put the complete way to able this window too.Thanks.