cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple discovery boards?

lee23
Associate II
Posted on June 09, 2015 at 19:26

I can load the Windows USB driver (into a VM--I don't oen any actual Windows box), and plug in a discovery board and all is well. Can update firmware, load stuff, etc. But when I try to connect another apparently identical board, I get a USB ''device not recognized'' error. Should I be able to connect more than one board? I can program them with st-link under Linux, but there are some things the Windows GUI thing would be handy for.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 09, 2015 at 19:38

Probably have different serial numbers and Windows wants to instantiate each individually. Each unique USB device gets it's own node in the registry.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..