2017-12-07 1:55 AM
NRST
� I/O Reset - Device reset input/internal reset output(active low). How can I connect this to a HC-05 bluetooth module?#stspin32f0a #bluetooth #nrst-pin #hc-052017-12-07 3:22 AM
A piece of wire should suffice?
What is it that you're actually asking? What is unclear?
2017-12-08 3:27 AM
Hello. If I want to reset the MCU using wireless serial interface, can I connect the NRST pin to the state pin of the HC-05 module? If not, what is the connection made? Thanks in advance.
2017-12-08 3:37 AM
The MCU will reset when NRST is pulled low - as described in its Datasheet and User Manual.
The MCU neither knows nor cares what causes NRST to go low - you can use any device which meets the requirements stated in the above-mentioned documentation.