cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Nucleo pack for IoT node with Wi-Fi: P-NUCLEO-CLD1

apfel sine
Associate
Posted on December 07, 2017 at 14:58

I like to start a new project based on the STM32Nucleo pack for IoT node with Wi-Fi(STM32 Nucleo-64 development board with STM32F401RE MCU).

I need to show some decimal values through a LCD keypad display. Here is my question, which LCD keypad display is the most suitable for the P-Nucleo-CLD1 board? Considering that I am not an expert I would like to use a display for which there are already libraries and how-to guides.

Any suggestions are appreciated.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal
Posted on December 08, 2017 at 13:50

You could use the same display as in the STM32 power shield. It's 2x16 characters, and you send ascii codes to the display by bitbang IO (small payloads).

Something like the one attached (transflecsive = can work without backligth for low power).

Don't have cube code example for it.

________________

Attachments :

NHD-C0216CZ-FSW-FBW-3V3.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyGK&d=%2Fa%2F0X0000000b58%2FtGbatQ.v1YqYv0g.c2Wk6iJ.FOz31Up0fuK1GiGS_6w&asPdf=false

NHD-C0216CZ-NSW-BBW-3V3.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyBu&d=%2Fa%2F0X0000000b5A%2F4XmcYGB0InudhhIOBCdvAK4R2nVzW6lWq9b91mlIswc&asPdf=false