2012-05-15 8:13 AM
i've faced a couple of problems, trying to launch a MT9D111 camera along with STM32F217ZG microcontroller through DCMI interface.
I've got all the interrupts from DCMI, but i can't catch any interrupt from DMA, although in the debugger window i can see that it is writing some thing into the buffer. May be you have seen this before. What can cause such a behaviour. I'm adding the initialisation code for dma interrupts. DMA_ITConfig(DMA2_Stream1, DMA_IT_HTIF1, ENABLE); DMA_ITConfig(DMA2_Stream1, DMA_IT_TCIF1, ENABLE); DMA_ITConfig(DMA2_Stream1, DMA_IT_TEIF1, ENABLE); DMA_ITConfig(DMA2_Stream1, DMA_IT_FEIF1, ENABLE); DMA_ITConfig(DMA2_Stream1, DMA_IT_DMEIF1, ENABLE); // Enable the DMA Stream IRQ Channel NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);2012-05-15 11:27 AM
Thoughts of the top of my head :
The DMA2 clock isn't enabled? The interrupt routine's name doesn't match the one in the vector table? DMA2_Stream1_IRQHandler() You're supposed to use the DMA_ITConfig(DMA2_Stream1, DMA_IT_TC, ENABLE); form? Not DMA_IT_TCIF12012-05-15 12:02 PM
Thank you, the last one helped.