cancel
Showing results for 
Search instead for 
Did you mean: 

Noise error with IrDA

dpereverzoff
Associate II
Posted on November 04, 2008 at 12:59

Noise error with IrDA

1 REPLY 1
dpereverzoff
Associate II
Posted on May 17, 2011 at 12:50

Seeing that the SIR of IrDA is 3/16 (or less for low power mode)bit period then is the Noise Error (NE) a valid test for the IrDA reciever?

If not, is there a way to disable this interrupt and still have interrupts for the other errors Overrun and Framing ?

I am using the DMA and do not want to check every character.