2014-07-10 12:11 AM
Hi
I have stm32f4 discovery board, first I could program the board but now It does not work. all jumpers are fine and I'm trying to run a sample program such as LED toggle. I checked the GPIO configuration and I just configure PA.4 for toggling. and this is my simple code:GPIO_InitTypeDef GPIO_InitStructure;int main(void){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); while (1) { GPIOA->BSRRL =GPIO_Pin_4; GPIOA->BSRRH =GPIO_Pin_4; }} then I tried to reset the board with pulling BOOT0 high. for this purpose,I connected BOOT0 pin to 3v pin. but It does not work yet. I'm working with Keil uvision 4 and It seems that keil can not recognize the ST Link,there is an error in options for target->Debug->ST Link Debugger ->setting : no ST Link detected.what should I do? please help methanks2014-08-06 5:13 AM
Hi Sahar,
Check with ST-Link Utility if your device is detected or not. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.