cancel
Showing results for 
Search instead for 
Did you mean: 

No output PWM for slave TIM channel

OW1TY2
Associate II

The MCU used is STM32F103VET6.

 

I want to use TIM3_CH1 (generating a PWM signal of 10kHz, 30% duty cycle) as the master input of TIM4_CH1. The TIM3 acts as the prescalar of TIM4 and thus making TIM4 to ouput a PWM signal of 200Hz and 60% duty cycle.

 

The below is my configuration of TIM4_CH1 in CubeMX and the code generated for initializing TIM3_CH1 and TIM4_CH1:

OW1TY2_0-1710063630371.png

static void MX_TIM3_Init(void)

{

 

/* USER CODE BEGIN TIM3_Init 0 */

 

/* USER CODE END TIM3_Init 0 */

 

TIM_ClockConfigTypeDef sClockSourceConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};

TIM_OC_InitTypeDef sConfigOC = {0};

 

/* USER CODE BEGIN TIM3_Init 1 */

 

/* USER CODE END TIM3_Init 1 */

htim3.Instance = TIM3;

htim3.Init.Prescaler = 0;

htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

htim3.Init.Period = 799;

htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;

if (HAL_TIM_Base_Init(&htim3) != HAL_OK)

{

Error_Handler();

}

sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)

{

Error_Handler();

}

if (HAL_TIM_PWM_Init(&htim3) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

sConfigOC.OCMode = TIM_OCMODE_PWM1;

sConfigOC.Pulse = 240;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN TIM3_Init 2 */

 

/* USER CODE END TIM3_Init 2 */

HAL_TIM_MspPostInit(&htim3);

 

}

 

/**

* @brief TIM4 Initialization Function

* @PAram None

* @retval None

*/

static void MX_TIM4_Init(void)

{

 

/* USER CODE BEGIN TIM4_Init 0 */

 

/* USER CODE END TIM4_Init 0 */

 

TIM_SlaveConfigTypeDef sSlaveConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};

TIM_OC_InitTypeDef sConfigOC = {0};

 

/* USER CODE BEGIN TIM4_Init 1 */

 

/* USER CODE END TIM4_Init 1 */

htim4.Instance = TIM4;

htim4.Init.Prescaler = 0;

htim4.Init.CounterMode = TIM_COUNTERMODE_UP;

htim4.Init.Period = 49;

htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim4.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

if (HAL_TIM_Base_Init(&htim4) != HAL_OK)

{

Error_Handler();

}

if (HAL_TIM_PWM_Init(&htim4) != HAL_OK)

{

Error_Handler();

}

sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;

sSlaveConfig.InputTrigger = TIM_TS_ITR2;

if (HAL_TIM_SlaveConfigSynchro(&htim4, &sSlaveConfig) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

sConfigOC.OCMode = TIM_OCMODE_PWM1;

sConfigOC.Pulse = 40;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

if (HAL_TIM_PWM_ConfigChannel(&htim4, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN TIM4_Init 2 */

 

/* USER CODE END TIM4_Init 2 */

HAL_TIM_MspPostInit(&htim4);

 

}

 

 

After that I just simple use the following codes:

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);

HAL_TIM_PWM_Start(&htim4, TIM_CHANNEL_1);

The TIM3_CH1 did generated the desired waveform but no ouput waveform was found on the pin PB6, is it because there are some connections has to be made on hardware level? Or simply because I should not use HAL_TIM_PWM_Start for TIM4_CH1?

 

PS. The reason I'm not using the default PB12 as the output of TIM4_CH1 is that PB12 was assigned as the backlight of the on-board LCD, I can't use it conveniently. 

1 REPLY 1

> want to use TIM3_CH1 (generating a PWM signal of 10kHz, 30% duty cycle) as the master

and then

> sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

I don't use Cube/HAL so I am not sure what the following line exactly means, but IMO it does not mean "set TIM3_CR2.TS to 0b100, i.e use CH1 as TRGO".

> no ouput waveform was found on the pin PB6

Can you see PWM output on that pin if you don't set TIM4 to be a slave?

> The reason I'm not using the default PB12 as the output of TIM4_CH1

PB12 does not have a TIM4_CH1 as output. PD12 does, but it's not the default - the default is PB6, see description of AFIO_MAPR.TIM4_REMAP in RM0008.

JW