2013-08-08 10:23 AM
hi all.. i'm already searching for hours, and can not find a working example / tutorial for SPI Slave on STM32F0. Anyone ?
thanks before... #need-stm32f0-spi-slave-tutorial2013-08-08 10:43 AM
Doesn't
\STM32F0xx_StdPeriph_Lib_V1.0.0\Project\STM32F0xx_StdPeriph_Examples\SPI\SPI_TwoBoards\DataExchangeInterrupt\main.c have a Master and Slave build configuration?2013-08-08 06:27 PM
Clive1, thanks for the quick response, but.. where is ''\STM32F0xx_StdPeriph_Lib_V1.0.0\Project\STM32F0xx_StdPeriph_Examples\SPI\SPI_TwoBoards\DataExchangeInterrupt\main.c'' ?
I'm using CooCox, there are no such file...edit: Clive1 point me the location ''\STM32F0xx_StdPeriph_Lib_V1.0.0\Project\STM32F0xx_StdPeriph_Examples\SPI\SPI_TwoBoards\DataExchangeInterrupt\main.c Has a Master and Slave build configuration?Don't know where the library code is? Try here thanks clive1... you are very helpful !!2013-08-09 12:18 AM
You can find it here http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257884
2013-08-09 06:58 AM
@ Edje : Thanks .... !!