cancel
Showing results for 
Search instead for 
Did you mean: 

Need Guide lines to start

angela15sruthi
Associate II
Posted on May 21, 2012 at 06:32

Hello all,

Am new to this controller and i have F0-discovery kit with. In the data brief preliminary document of the kit it is mentioned as follows:

2           Development toolchains

â—�       Altium TASKINGâ„¢ VX-Toolset

â—�       Atollic TrueSTUDIO®

â—�       IAR, EWARM

â—�       Keilâ„¢, MDK-ARM

Can any one please suggest which is the best tool to start? and any help documents or application notes (if any to start). Any other suggestions from the experts are most welcome . I am awaiting for a better future with this controller. Thanks!!!!!!good day :)

NOTE: please reply asap. I am sorry to say that the STM customer support is worst and i didnt get any reply from them, almost a week am waiting for the reply. I have the kits and tools. But waiting for the reply to start.
13 REPLIES 13
jlchoobs
Associate II
Posted on June 14, 2012 at 09:45

I don't actually see much if any useful code being posted in this forum.

But I atleast can provide some of my own :

 

[[this link/image has been flagged as malicious by our security scan software and has been deleted]]

I am also working on (and hope to post soon) a port of the stm3240g Firmware over to the stm32f4discovery board. 

frankmeyer9
Associate II
Posted on June 14, 2012 at 16:53

You try hard to provoke me.

Why don't you go 

[[this link/image has been flagged as malicious by our security scan software and has been deleted]]

 to live out your god complex ?

Posted on June 14, 2012 at 20:20

''Keil ... is a PAIN to Debug - their own Headers Lib so you have to buy their product :(=''

 

Please would you explain what you mean by that?

It is certainly possible to build, download, and debug projects for STM32 Discovery boards using only the free Keil download (''MDK Lite'') with no need to purchase anything else.

Within the stated limits, of course:

http://www.keil.com/demo/limits.asp

ST provide example workspaces for Keil and IAR in the Discovery board downloads;

ST provide example workspaces for Keil, IAR, HiTOP, RIDE, and Atollic in the Standard Peripheral Library download.

Of course, you can buy proprietary libraries from Keil if you wish - but it is by no means essential.

robertpapp9
Associate
Posted on July 26, 2012 at 01:00

Hi,

As I had good experiences with LPCxpresso, which is an Eclipse based IDE, installed and evaluated Atollic (TrueSTUDIO for ARM Lite 3.1.0)  and Tasking (TASKING VX-toolset for ARM Cortex v4.2r1) at first. The results are disappointing: bugs,compiler errors, other strange error messages or at least code size limit error when trying  STM32F4-Discovery examples.

Than installed IAR 6.4 Kickstart Edition which works fine.

No experiences with Keil for STM32 (  for developing firmware on Luminary Micro was a pleasure some years ago...)

For the first two, finding information on the web in case of a problem is not an easy task.

IAR and Keil are two, experienced companies providing tools for microcontrollers, which means less bugs, more information about their products. I recommend using their toolchains.

Regards,

Robert