‎2019-06-10 10:05 AM
Hi!
I'm a newbie to all of this. I purchased an STM32F1038C8T6 development board or "Blue Pill" recently.
I connected it to my PC Windows Using a Usart to serial converter.
I read that I should put one of the BOOT Jumpers in the one position to enter programming mode. I did that and reset the module, but PC13 won't stop blinking. I tried all combinations of boot jumpers but nothing stopped the blinking led. So I got over this put it in programming mode (PC13 Still Blinking rapidly) and tried to upload a sketch. I get the message that it failed to init the device.
Spent a week trying to solve this but to no avail.
Please help
Regards
Kamal Ayoub
‎2021-05-28 08:59 PM
Removing the registers Worked fine for me as well
‎2021-08-08 05:35 AM
Thank you for the tip. removed 100K @ R3 and made it direct. Worked for me.
‎2022-10-31 06:12 PM
This worked, Thanks bro!!
‎2022-10-31 06:13 PM
Works like a charm =)
‎2022-10-31 06:14 PM
Thank u for your help bro :oncoming_fist: