2025-03-06 12:59 PM
Hello, I am using the B-U585-IOT02A board with Zephyr. I can't see how to use the MXCHIP EMW3080 Wi-Fi chip. Has anyone made this work? Thanks
2025-03-07 1:02 AM
Hello @stuart_rubin_ns,
for the WIFI module: you can get the firmware on this link and then follow the procedure describe in the UM to program the WIFI module.
Also, you can find more details in the datasheet provided by MXCHIP: EMW3080-DS0069EN.pdf
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-07 10:10 AM
Sarra, thank you for your reply. Unfortunately, my issue is specifically with using Zephyr. This board (B-U585-IOT02A) does have Zephyr support, but it's not obvious for how to use Wi-Fi with Zephyr. Do you have any information on that? Thank you.
2025-11-25 6:11 AM
Hi Stuart. Did you manage to get this working under Zephyr? I am using the STMH7S78-DK board and want to use WiFi with the MXCHIP EMW3080 but stubbed against the same wall as you. Thanks in advance.