2018-05-08 2:43 PM
I am confused over the inability to successfully setup an MPU region for the area that the DMA is using. I am trying to get around having to use Clean and Invalidate Cache like so to guaranty the data is passed correctly:
SCB_CleanDCache_by_Addr((uint32_t *)EclFrame, ((BytesToSend+31)/32)*32); //works
result = HAL_UART_Transmit_DMA(&UartHandle, (uint8_t *) EclFrame, BytesToSend);
and:
result = HAL_UART_Receive_DMA(&UartHandle, (uint8_t *)EclFrame, BufferSize);
SCB_InvalidateDCache_by_Addr((uint32_t *)EclFrame, ((BufferSize+31)/32)*32); // works
I have tried to setup a region for RAM_D1 like so:
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x24000000; MPU_InitStruct.Size = MPU_REGION_SIZE_512KB; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; //also tried NOT MPU_InitStruct.Number = MPU_REGION_NUMBER4; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.SubRegionDisable = 0x00; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;HAL_MPU_ConfigRegion(&MPU_InitStruct);
with the result being that the transmit sends the wrong data. I am not sure about receive since this is used in a command-response sequence hence sending the wrong data out means no data back. There are three other memory regions setup and they are working fine so I do not get why this region should have a problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.