cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Pilot 6.3.2 wont connect to STM32 MCU board

Tedco
Associate II

Downloaded the STM32Cube Motor Control SDK and installed the app which came up as ``Motor Pilot 6.3.2`.

I connected the STM32 MCU board (B-G473E-ZEST1S) via USB to my desktop.

When I launch the program it looks like this:

Tedco_0-1744411044509.png

It shows that there is ``No Connection`` to the board and the only option is for a UART on com3 or com4. When I try com3 and press Connect, the program closes.

Any help would be greatly appreciated!

Barry

Tedco Electric

 

 

 

1 REPLY 1
GMA
ST Employee

Hello @Tedco,

You can try the "Discover Board" feature available on MC Pilot>GUI>"Reset GUI to Default".

Refer to "Getting Started with Motor Control SDK" chapter in "Workbench tool">About>Documentations>Documentation".

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA