2014-08-04 1:28 AM
How can I try the Nucleo board with a Keil. It reports a missing target ...411. Why that?
#keil #nucleo #stm32f4112014-08-04 3:23 PM
If you've installed all of the assorted packs and legacy stuff, your next stop should be support@keil.com
http://www.keil.com/support/contact.asp
http://www.keil.com/arm/chips.asp
Pretty sure you could pick a similar STM32F4 device and tweak the memory map, defines, etc and get it to compile.2014-09-15 8:11 AM
I am having a similar problem. Shouldn't this be in place before the product is released. Which micro is closest? STM32F407? F401? F415?
2014-09-15 9:21 AM
I am having a similar problem. Shouldn't this be in place before the product is released.
I'm sure it is, have you spoken to your TOOL vendor? There's usually a patch or architecture file, and it would probably also be available to commercial ST clients through the normal support structures, ie reps and FAEs The Nucleo board target mbed2014-09-30 9:52 AM
Hi joee,
if you are using an existing project, settings can not be lost and you will be able to compile/run it. if you have created a new project, you can not select STM32F411 device since it is not yet supported. Best Regards, Nouha