cancel
Showing results for 
Search instead for 
Did you mean: 

Migrate from STM32F103 to STM32F413

JHeni
Associate II

0690X000008A6bNQAS.pngHey guys,

I'm currently migrating a STM32F103 project to an STM32F413 project using CubeMX.

I created a new STM32F413 Cubemx project and imported the old STM32F103 project. Most settings were successfully mapped to the new MCU.

However since the F1 has 3 ADCs and the F4 only 1 i'm currently stuck at migrating the ADCs.

In my old project I used ADC3 IN4 and IN5 (on PF6 and PF7) to convert an analog touch input. However when I tried to configured PF6 and PF7 as an Analog Input I could not find the ADC settings.

The only settings for these Pins available are (see ataached File).

However STs migration guide F1 to F4

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/e9/c4/6b/99/4e/d3/4e/a0/DM00325582/files/DM00325582.pdf/jcr:content/translations/en.DM00325582.pdf

states in Table 7 full ADC compatibility (see Atached file).

So for my understanding, the F1 ADC pinout is complately the smae as the F4 ADC Pinout. So what am i missing?

Could you give me a hint please.

0 REPLIES 0