2012-05-31 03:27 AM
Hi,
does anybody use the MicroXplorer Eclipse plugin with Linux and Eclipse 3.7?Here it either crashes Eclipse or I can't choose an MCU.Moritz #microxplorer-ubuntu64-crashes2012-09-06 02:06 PM
Mine also cannot operate,
using Ubuntu 64 with Eclipse Indigo, the following eclipse.ini at least and at last got me opening all: -startup plugins/org.eclipse.equinox.launcher_1.2.0.v20110502.jar --launcher.library plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505 -showsplash org.eclipse.platform -vm /usr/lib/jvm/java-7-oracle/jre/bin/java --launcher.XXMaxPermSize 2048m --launcher.defaultAction openFile -vmargs -Xms128m -Xmx2048m All else is well.But if I stretch the MicroXplorer menu open, it crashes. [I pull the separation bar up so that the blue MicroXplorer icon get larger]
Before it crashes - I also cannot select MCU's
I tried everything I could find on the net. [I did install everything the proper way] Tired, Desperate...2012-09-06 11:34 PM
System
It is an Intel MB, 16Gig RAM, Quad Processor Nvidea graphics2012-09-06 11:35 PM
UBUNTU error report:
The crashed program seems to use third-party or local libraries: /home/za/eclipse/plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505/eclipse_1407.so /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-gtk-3740.so /home/za/eclipse/configuration/org.eclipse.osgi/bundles/84/1/.cp/os/linux/x86_64/libunixfile_1_0_0.so /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-atk-gtk-3740.so /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-pi-gtk-3740.so /home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-cairo-gtk-3740.so It is highly recommended to check if the problem persists without those first.What do I do with this?