Microcontroller stucks when uart not connected
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-08-27 9:23 PM
i am using stm32L072
I am using uart1 in the code
I found that code doesn't works ,if i don't connect a usb to uart converter between PC and the microcontroller .
When i connect usb to uart connector and reset microcontroller ,it starts working :weary_face: or if i comment uart_init function ,the code works fine without usb-uart converter .
What might be the issue ?
Below is uart initialization code :
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* (1) Enable GPIO clock and configures the USART pins *********************/
/* Enable the peripheral clock of GPIO Port */
USARTx_GPIO_CLK_ENABLE();
/* Configure Tx Pin as : Alternate function, High Speed, Push pull, Pull up */
LL_GPIO_SetPinMode(USARTx_TX_GPIO_PORT, USARTx_TX_PIN, LL_GPIO_MODE_ALTERNATE);
USARTx_SET_TX_GPIO_AF();
LL_GPIO_SetPinSpeed(USARTx_TX_GPIO_PORT, USARTx_TX_PIN, LL_GPIO_SPEED_FREQ_LOW);
LL_GPIO_SetPinOutputType(USARTx_TX_GPIO_PORT, USARTx_TX_PIN, LL_GPIO_OUTPUT_PUSHPULL);
LL_GPIO_SetPinPull(USARTx_TX_GPIO_PORT, USARTx_TX_PIN, LL_GPIO_PULL_UP);
/* Configure Rx Pin as : Alternate function, High Speed, Push pull, Pull up */
LL_GPIO_SetPinMode(USARTx_RX_GPIO_PORT, USARTx_RX_PIN, LL_GPIO_MODE_ALTERNATE);
USARTx_SET_RX_GPIO_AF();
LL_GPIO_SetPinSpeed(USARTx_RX_GPIO_PORT, USARTx_RX_PIN, LL_GPIO_SPEED_FREQ_LOW);
LL_GPIO_SetPinOutputType(USARTx_RX_GPIO_PORT, USARTx_RX_PIN, LL_GPIO_OUTPUT_PUSHPULL);
LL_GPIO_SetPinPull(USARTx_RX_GPIO_PORT, USARTx_RX_PIN, LL_GPIO_PULL_UP);
/* (2) NVIC Configuration for USART interrupts */
/* - Set priority for USARTx_IRQn */
/* - Enable USARTx_IRQn */
NVIC_SetPriority(USARTx_IRQn, 0);
NVIC_EnableIRQ(USARTx_IRQn);
/* (3) Enable USART peripheral clock and clock source ***********************/
USARTx_CLK_ENABLE();
/* Set clock source */
USARTx_CLK_SOURCE();
/* (4) Configure USART functional parameters ********************************/
/* Disable USART prior modifying configuration registers */
/* Note: Commented as corresponding to Reset value */
// LL_USART_Disable(USARTx_INSTANCE);
/* TX/RX direction */
LL_USART_SetTransferDirection(USARTx_INSTANCE, LL_USART_DIRECTION_TX_RX);
/* 8 data bit, 1 start bit, 1 stop bit, no parity */
LL_USART_ConfigCharacter(USARTx_INSTANCE, LL_USART_DATAWIDTH_8B, LL_USART_PARITY_NONE, LL_USART_STOPBITS_1);
/* No Hardware Flow control */
/* Reset value is LL_USART_HWCONTROL_NONE */
// LL_USART_SetHWFlowCtrl(USARTx_INSTANCE, LL_USART_HWCONTROL_NONE);
/* Set Baudrate to 115200 using APB frequency set to 16000000 Hz */
/* Frequency available for USART peripheral can also be calculated through LL RCC macro */
/* Ex :
Periphclk = LL_RCC_GetUSARTClockFreq(Instance); or LL_RCC_GetUARTClockFreq(Instance); depending on USART/UART instance
In this example, Peripheral Clock is expected to be equal to 16000000 Hz => equal to SystemCoreClock
*/
LL_USART_SetBaudRate(USARTx_INSTANCE, SystemCoreClock, LL_USART_OVERSAMPLING_16, 115200);
/* (5) Enable USART *********************************************************/
LL_USART_Enable(USARTx_INSTANCE);
/* Polling USART initialisation */
while((!(LL_USART_IsActiveFlag_TEACK(USARTx_INSTANCE))) || (!(LL_USART_IsActiveFlag_REACK(USARTx_INSTANCE))))
{
}
/* Enable RXNE and Error interrupts */
LL_USART_EnableIT_RXNE(USARTx_INSTANCE);
LL_USART_EnableIT_ERROR(USARTx_INSTANCE);
/* USER CODE END USART1_Init 0 */
Labels:
- Labels:
-
STM32L0 Series
-
UART-USART
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0