2023-05-10 2:18 AM
Hi, i'm working on a custom board with a stm32F746VGT6. After many succesfull programming attempt an error occurred (see the image attached to the question).
With the tool "Stm32CubeProgrammer" i can connect to the board and program it, but only with a selected frequency of 5KHz.
I've already tried to reset the Option byte and do a mass erase of the micro.
How can i solve?
Thanks
2023-05-10 2:53 AM
Other times the IDE fails to finish the flash operation and print out this message in the console:
STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.13.0
-------------------------------------------------------------------
Log output file: C:\Users\ricca\AppData\Local\Temp\STM32CubeProgrammer_a07868.log
ST-LINK SN : 003900213331510E34333834
ST-LINK FW : V3J10M3B5S1
Board : STLINK-V3SET
Voltage : 3.28V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 003900213331510E34333834
ST-LINK FW : V3J10M3B5S1
Board : STLINK-V3SET
Voltage : 3.29V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Encountered Error when opening C:\ST\STM32CubeIDE_1.11.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.