2024-10-25 09:13 AM - last edited on 2024-10-25 10:16 AM by Imen.D
Hello,
please mention RCC_BDCR_LSESYSEN in U0 reference manual in the LCD chapter. This is a new requirement when running LCD with LSE on STM32U series. Maybe chapter with other devices to run on LSE clock will profite too.
Regards
2024-10-25 10:12 AM - edited 2024-10-25 10:16 AM
Hello @Uwe Bonnes
Thank you for noticing it.
An internal ticket (number 195086) is submitted in order to improve the STM32U0 reference manual.
(PS: This is an internal tracking number and is not accessible or usable by customers).