2020-10-09 1:11 AM
Hi, I am looking for MCU which support 1.8 V GPIO and 3.3 V GPIO,
My target is about 20 pin 1.8 V GPIO and about 10 pin 3.3 GPIO.
After my search, I think STM32F0x8 can meet my requirement.
I want to know are there STM32 low power series MCU or STM32 High Performance MCUs
can also meet my requirement?
Flash need > 128K, RAM need > 20K. It's better to have USB.
Thanks
Ken
2020-12-04 12:42 PM
You can check the STM32L552, which is providing a separate pin VDDIO for exactly that purpose, 256KB or 512KB Flash, 192+64KB RAM and USB 2.0 Device FS Crystal Less.
Regards
/Peter
2020-12-04 1:16 PM
The L4+ parts has a GPIOG bank that can be powered independently via a VCCIO pin