cancel
Showing results for 
Search instead for 
Did you mean: 

MCU : stm32h743ii. two usart problem

RLiu.11
Associate II

i use two uart.(usart1 & usart2).

when i receive data(usart1), first, the program will into

"void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)".

but when i i receive data(usart2), second, the program will not into

"void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)".

is it bug ???

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

Check the whole interrupt chain, from USART registers' content through NVIC registers, address of the real ISR being inserted properly into the vector table, the real ISR containing proper redirection to Cube's USART ISR handler, etc.

JW

TDK
Super User

Hard to know for certain. Perhaps it isn't configured correctly. Perhaps you are not actually receiving data. Perhaps you are receiving data but the clock rate is wrong so it's going to the error handler instead.

If you feel a post has answered your question, please click "Accept as Solution".

>>is it bug ???

No, it provides you with the instance/context of the UART involved. You could perhaps overload the structure, adding you own on the back-end to carry buffers, or state variables.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..