cancel
Showing results for 
Search instead for 
Did you mean: 

maximum spi clock for spi slave in STM32F030 at slow fclk clock?

Tamas Novak
Associate III
Posted on March 18, 2015 at 18:06

Is there a maximum ratio of FCLK and external SPI clock?

I use STM32F030 with SPI module as slave. What is the maximum external SPI master clock?  I'd use low speed clock at my STM32  (HSI 8MHz, or maybe HSI+PLL devided down to 1MHz FCLK). What is the maximum external SPI master clock in this situation?

#stm32f030-spi-clock
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0