2026-06-03 1:06 AM - last edited on 2026-06-04 1:55 AM by Andrew Neil
Hello everyone, may I ask what is the maximum clock frequency supported when the STM32H7's FMC peripheral controls SDRAM? Can it work stably if the frequency exceeds 200MHz, for example, 240MHz?
Thank you very much.
Solved! Go to Solution.
2026-06-03 1:15 AM - edited 2026-06-03 1:17 AM
Hello,
That depends on which STM32H7 you are talking about. You should always provide the MCU part number you are referring tor.
For STM32H74x , it's provided in the RM0433 / Table 55:
2026-06-03 1:15 AM - edited 2026-06-03 1:17 AM
Hello,
That depends on which STM32H7 you are talking about. You should always provide the MCU part number you are referring tor.
For STM32H74x , it's provided in the RM0433 / Table 55:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.