cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 FMC_CLK output

Mark_22
Visitor

Hello,

I am interfacing an FPGA with a STM32H742 and plan to use a mux'd bus,  synch mode and PSRAM memory type.  I will have two banks,  one with 16bit data,  one with 8bit data.  To simplify the FPGA interface I would like to use the FMC_CLK output in continuous mode.  There is a warning that the FMC_CLK frequency can change based on the AXI data size and the memory interface.   Is there a way to prevent the FMC_CLK frequency change?    Would the FMC_CLK frequency remain the same if my program accesses all data in the 16bit bank as 16 bit variables and accesses all data in the 8bit bank as 8 bit variables.   Note that most of the access to the 8bit bank will be performed using DMA.

Thank you.

 

0 REPLIES 0