2018-01-30 3:11 PM
When i plug in my STM32 Nucleo-f303k8 windows detects it as a mass storage device. Is there any way to write data in this memory from the ucontroller?
2018-01-31 8:59 AM
There was a long discussion about this a couple of months ago - IIRC, the conclusion was, 'No.'
The mass storage that you see is for the mbed bootloader.
2018-01-31 9:26 AM
The ST-LINK is faking a MSC, you can write a binary that replaces the entire memory content of the target device. This is how the mbed drag-and-drop programming works.
2018-01-31 10:13 AM
Can you link me that post please?
2018-01-31 10:23 AM
The forum is currently in a semi-broken state, providing directly links fails in most cases and for many users.
The flash arrangement and speed of write/erase is not conducive to real-time operation and management of 512 byte block devices. Erase and Write will stall the processor when running code from flash.
2018-01-31 10:51 AM
I would have but, as
Turvey.Clive.002
says, the forum is not currently in a fit state.Sorry.
:(