cancel
Showing results for 
Search instead for 
Did you mean: 

The “Virtual Port Comm” issue on STM32F407

No_Name
Associate III

Hi everyone.

I tried adding USB_OTG_FS/Virtual Port Comm to STM32F407VET6 as a device only, but the problem is that when I try to connect the STM32 USB to my PC/laptop, it says “USB not recognized” on my PC/laptop, and I think it might be a problem with the cable, but after I replaced the cable 5 times and tried connecting it to my laptop, the problem remained the same.

Where does this problem originate—in the code or the hardware itself?

I used two boards, and both experienced the same problem.

 

images.jpegstm32f407vet6-mini-development-board-development-boards-motorobit-35797-34-B.jpg

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

I replaced the MCU on the board with the original MCU.

thank you :)

0 REPLIES 0