2024-07-11 12:25 PM
Hi, i'm trying to enable the tilt feature in an LSM6DSO on INT1 or INT2 but isn´t been possible until now. I´ve read the datasheet and used the example as template but for some reason the interrupt is not working. Looks like the embedded functions are not being activated correctly. These are the registers that I'm using to configure it. First hex is the register direction and the second one is the value to write.
2024-07-22 05:04 AM
Hi @Juandgarcia ,
Welcome to ST Community!
Have you already looked at our official example on Github?