2017-08-23 4:15 AM
Hello everyone,
I'm working on a LoRa project, using Murata's module ( stm32l082 & semtech's SX1276) , The aim of the project is to send some datas ( temperature, pressure .. ) to a gateway.
I want to know if someone has succeed to modify the example program given in I-CUBE-LRWAN 1.1.0 for B-L072Z-LRWAN1 in order to send datas without using the shield. Or there is any other solution ( code ) should i start with ?Thank you,
2017-08-24 6:03 AM
This code seems nice to ...
2017-08-24 7:51 AM
>>
Have you ever did a project like this before ?
Yes, it's my job.
2017-08-24 7:52 AM
Thank you for your advices Goran Mahovlic, actually i already past this step, i have a card with sensors connected in I2C, i need to modify the ST's provided code.
could you tell me please what are the exact modifications to do ?2017-08-24 7:58 AM
LoRa radios are exceedingly effective at point-to-point communication. You can also own both ends of the communication link, rather than deal with the complexity of a multi-channel gateway radio.
2017-08-24 7:59 AM
I use CubeMx and build only I2C sensor (or whatever you want) to get it work.
When that is working I just check what I need to copy paste into LoRa code...
2017-08-24 8:02 AM
Greaat (Y) !
because i was trying to modify the project, but i think it's a better idea, thank's.2017-08-25 5:04 AM
Hello,
i tried to build a new project but i didn't succeed, so i worked with the LRWAN_cube project with adding sensors ( I2C communication), and actually i receive something weird in gateway :{unexpected_data,{rxdata,0,2,<<'Hello word, STM32 i LoRaWAN connected'>>,false,true}}
Do you know why it's wrote : unexpected_data?
Thank you2017-08-25 5:05 AM
Hello,
I worked with the LRWAN_cube project with adding sensors ( I2C communication), and actually i receive something weird in gateway :{unexpected_data,{rxdata,0,2,<<'Hello word, STM32 i LoRaWAN connected'>>,false,true}}
Do you know why it's wrote : unexpected_data?
Thank you