2025-06-17 9:40 PM
Hi,
I am working on a lighting control project and looking for an STM32 evaluation board that supports native DALI interface.
By native support, I mean:
Does ST offer any evaluation boards or MCUs with these features built-in? Or would I need to implement DALI support entirely in software with an external transceiver?
Any suggestions or guidance would be appreciated.
Thanks and Regards,
Yaadesh S
2025-06-17 10:49 PM
NXP had one about a decade ago, but AFAIK they dropped it soon.
I think DALI is just a too specialized niche product to justify investment into development platforms, especially since it involves mostly the lowest-cost section of MCUs. I never came across any general-purpose MCU that natively supported a DALI interface. And basically all DALI products I had been working on at that time used low-cost 8-bit MCUs (MCP or Atmel).