cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for alternative STM32 peripheral libraries

Matt_12345
Associate II
Posted on June 12, 2014 at 16:11

Hi,

I'm in a project were we would like to use the STM32F103TBU7. As a toolchain we would like to use the IAR Embedded Workbench.

Sadly I'm not allowed to use the STM peripheral library. This because it's a security application and we have to use two different libraries.

Does somebody can give me a hint which library I could use?

We did already some tests with libopencm3 but this library is designed for the gcc compiler.

Thanks for your inputs

Matt 

#stm32-utasker
10 REPLIES 10
frankmeyer9
Associate II
Posted on June 18, 2014 at 08:48

AFAIK the Cortex R microcontrollers have most of the features you want.

I'm not aware of any such silicon by ST, but TI has such a series, called Hercules.